2022-10-01 4:09 AM
I'm trying to use the RX / TX interface on J5 on the B-G431B-ESC1.
However, it looks like the ST-LINK daughterboard uses those pins too.
I know I can snap off the daughterboard, but I still want to be able to use the ST MCSDK tools, switching back and forth as needed.
Unfortunately, a HW is a pain as the lines are simply shared and there's no good solder pads on the ST-LINK daughterboard and the ESC board to make a jumper.
What would be even better though, is being able to get the stm32 103 chip on the daughterboard to simply tri-state those lines when they are not being used.
If I don't power the daughterboard, the MCU drags the lines down too far, if I power through USB and / or 12v on the main + - pins for the motor and battery elimination circuit, then the 103 is actively trying to drive those lines, making the ones on J5 useless.
Any ideas?
Is there any way to do this?
Solved! Go to Solution.
2022-10-06 3:13 AM
Ciao
I'm looking the schematics of the board B-G431B-ESC1 but I see that the USART pin is mapped into J3 not in J5 (maybe is a typo).
Anyhow I think it is possible to unlink the USART pin of the main controller from the STLINK unsoldering these two resistors:
Ciao
Gigi
2022-10-06 3:13 AM
Ciao
I'm looking the schematics of the board B-G431B-ESC1 but I see that the USART pin is mapped into J3 not in J5 (maybe is a typo).
Anyhow I think it is possible to unlink the USART pin of the main controller from the STLINK unsoldering these two resistors:
Ciao
Gigi
2022-10-06 10:10 AM
Yes, J3, J5/J6 are the power input pins on either side of J3.
I'll have to see if I can find where those resistors are on the board, I'm sure they're very tiny.
2022-10-07 1:28 AM
R23 and R24 are easily found on the bottom side of the daughterboard:
Regards
/Peter