cancel
Showing results for 
Search instead for 
Did you mean: 

asking about steval-1sa170v1

AMIRA_BESHIEER
Associate II

Hello, where can i find the altium files for steval-1sa170v1?

17 REPLIES 17
Andrew Neil
Evangelist III

What makes you think that Altium files should be available?

https://community.st.com/t5/stm32-mcus-boards-and-hardware/altium-file-for-stm32f0discovery/m-p/629324/highlight/true#M16779

If you go to the Product Page for the board, schematics, etc, will be under 'CAD Resources'

AMIRA_BESHIEER
Associate II

The gerber files in CAD Resources is empty, so i think the layout and altium files can be available 

You're assuming that ST use Altium.

Other systems are available ...

AMIRA_BESHIEER
Associate II

ok, How can i open the gerber files in CAD resources?

  

I can't see a Product Page for "steval-1sa170v1" - can you give a link?

Thanks.

So I see Gerbers, BoM, and Schematics all available for download there:

AndrewNeil_0-1706093330272.png

The Gerbers download as a Zip; the BoM and Schematics as PDFs:

AndrewNeil_1-1706093493393.png

Inside the Gerbers Zip:

AndrewNeil_2-1706093563110.png

 

 

i couldn't open the gerber files. so i asked for the layout or what is the method to open it?

Peter BENSCH
ST Employee

Well, GERBER data is actually only intended for plotting a layout or producing a board, similar to PDF, which is also only intended for printing and not for re-layouting. However, you can use a GERBER viewer to orientate yourself on details from its data and derive your own layout. There are GERBER viewers that you can use for free, e.g. the one in the KiCAD package.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.