2013-09-19 08:43 AM
Hi Everybody
Im power my motor with 22 Volts with the following Register values:KVAL Register 0X10 (HEX) OC SD_ DISABLE = Do not schut down the bridges on overcurrentAs the voltage rises to 24V (in orden to obtain more Torque) the engine stops and lose its Torque.. I Just need to power again with 22V and the motor works Anybody knows what im doing wrong.. Why stops the motor exactly on 24 V?Thank you for your help #l6470-24-volts_-motor-stop2014-01-02 01:17 AM
CiaoEdgar
I suggest post this thread in the forum. Thanks Ciao Gigi