2025-10-14 12:08 AM - last edited on 2025-12-29 5:49 AM by ELABI.1
Hi everyone,
I’m working on a design using an STM32H7 MCU communicating with a GPS/GNSS module over UART. Unfortunately, during board routing, the RTS and CTS lines were connected directly (RTS↔RTS, CTS↔CTS) instead of crossed.
I understand that for proper hardware flow control, they should be:
STM32 RTS → GPS/GNSS CTS
STM32 CTS ← GPS/GNSS RTS
At this stage, I can’t modify the hardware or rework the PCB, but I’d still like to maintain some form of flow control or transmission reliability if possible.
2025-10-14 2:11 AM
Just drive them "manually" as GPIOs ?
Is XON/XOFF (so-called "software" flow control) supported?
@Muruganandam wrote:but I’d still like to maintain some form of flow control or transmission reliability if possible.
GNSS modules generally work fine without flow control ...