Skip to main content
KGane.1
Associate III
September 7, 2022
Question

IAR - Redirect printf to UART and fprintf to SD card FAT File system

  • September 7, 2022
  • 5 replies
  • 4156 views

I am using IAR EWARM 9.10.2 and would like to redirect printf to UART and fopen/fclose/fprintf to SD card hosting FAT File System(R0.12c (March 04, 2017)). Any guide on how to do redirect io streams on IAR would be helpful.

Thanks in advance.

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
September 7, 2022

https://wwwfiles.iar.com/arm/webic/doc/ewarm_developmentguide.enu.pdf

Is suspect you need to replace __write function with your own, or redirect the linker to use yours rather than it's own.

--redirect __write=__write_kgane

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KGane.1
KGane.1Author
Associate III
September 7, 2022

@Community member​ Thank you!.

I tried redirecting fpintf to SD card. I found templates for file operation in \IAR Systems\Embedded Workbench 9.0\arm\src\lib\file.

Implemented __open/__close/__write/__read/__/lseek. When running code in IAR debug mode, the execution trapped using BKPT instruction. Seems the IDE is semi-hosting.

0693W00000Suk27QAB.png 

0693W00000Suk22QAB.png

Tesla DeLorean
Guru
September 7, 2022

Perhaps a check-box item in the project/build metadata, or can be changed via a #pragma

Sorry, team Keil here, but I'd expect IAR would facilitate relatively easily

https://stackoverflow.com/questions/10503680/use-of-arm-semihosting

Some of the redirect examples talk of the buffered write, where you provide that functionality.

--redirect __write=__write_bufferred

https://www.iar.com/sv/knowledge/learn/programming/overriding-and-redirecting-library-modules-without-rebuilding-the-entire-library/

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
September 8, 2022

Just select a non-minimal variant of the IAR runtime library, that uses file handles (or descriptors).

Do not select semihosting, of course.

Then your _write replacement will receive the file handle/descriptor number.

Send the data for different descriptors to different destinations, as you like. Values 1 and 2 are stdout and stderr.

KGane.1
KGane.1Author
Associate III
September 9, 2022

@Community member​ , @Pavel A.​ Thank You.

I can redirect to both UART and SD Card using "Full" Library Configuration. I had to disable "Buffered terminal output" in IAR. In addition to own implementation of __open/__close/__write/__read/__/lseek, putchar and getchar needs modification to call to UART TX & RX functions.

The following TN is useful.

https://www.iar.com/knowledge/support/technical-notes/compiler/migrating-projects-with-the-custom-fputc-function/