2026-05-24 6:08 AM - last edited on 2026-05-26 1:51 AM by Andrew Neil
Split from BNO085 not working with STM32L433RC-P nucleo board - which appears abandoned.
Any update on this I am facing the same issue , did your issue got resolved if yes 1) at how uch frequency BNO085 is giving you the output and also can u please share your code and repo
2026-05-24 11:33 PM
can u please explain what do you mean by sequence handling
2026-05-26 2:00 AM - edited 2026-05-26 3:08 AM
welcome to the forum
Rather than hijack someone else's old, abandoned thread it's better to start your own - then you will be able to mark the solution when the problem is resolved (only the person who started a thread can do that).
Please provide a full description of your actual setup, and what investigation/testing/debugging you have done so far -
see: How to write your question to maximize your chances to find a solution for best results.
Have you followed the suggestions given in the old thread?
@dinesh_ee_bme_72 wrote:can u please explain what do you mean by sequence handling
Not sure what you mean by that - I don't see "sequence handling" anywhere in the other thread ?
Are you referring to where @DUBEYISM said, "I also attempted different initialization sequences and delays, but the sensor remains unresponsive on STM32" ?
PS:
Is this the same issue here: BNO085 I2C with STM32H7A3 via SH2 library — stuck at 44Hz but ESP32 achieves 1.2ms read time ?