2004-02-01 8:58 PM
Where can I find how to make a .mak and a .lkf file?
2004-01-18 6:09 PM
Hello.
Nice to see you here. I want to know how to handle and make a .mak file and a .lkf file. Can I find them somewhere? I will be obliged to you, If you would teach. [ This message was edited by: musu on 19-01-2004 07:42 ] [ This message was edited by: musu on 19-01-2004 07:57 ]2004-01-20 4:21 PM
you can find sample workspace in toolchain directory
c:\Program Files\STM\stst7toolchain\stvd7\emu3\samples Which device and compiler you are using?? Hope this help Regards, PraveenG2004-01-20 4:34 PM
You can also find it with the software codes attached with the various application notes and ST7 software library available on this same site. You have to configure certain parameters(like for example: Compiler options, memory model, Start Address etc) in .mak & .lkf files depending up on your application.
2004-01-20 8:43 PM
Hi Musu,
a .mak file recompiles your application if it detects that one (or more) of the source or intermediate files has been saved later than the executable file. In it, you define the conditions for compiling, linking or both. A .lkf file, is the linker file you use for link your project. I've attached a working example (for ST72F521) made with STVD7 and Cosmic compiler. I hope this could help you. Cheers! [ This message was edited by: Nicola on 21-01-2004 10:14 ] ________________ Attachments : 521.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I074&d=%2Fa%2F0X0000000bTb%2FxfiYDIfLf393ZwJerSt4GW.Z12oc6ML4M8t1VgmdSTw&asPdf=false2004-01-25 1:50 PM
I'm very sorry.
In my first query, I should describe my development kit. But I didn't. My one is Cosmic C compiler & STVD7 (Indart ST7). And I really feel a thank all of you for the kind answering.2004-01-25 2:02 PM
I've losted describing my develop tools (STVD7 of Indart) & compiler (Cosmic C).
I really feel a happy. Thank all of you for the kind answering. And Mr. Nicola Sir. Are you an Itaian? I like the Juventus. It's my vest favorite soccer team in the world. Nedved & Del Piero.... they are awesome.2004-02-01 8:58 PM
Hi Musu,
Yes, I'm Italian, I'm surprised you are a Juventus fan!!! Unfortunately I'm a Milan fan, but I think Juventus is a great team too!!! Regads.