2021-05-09 12:44 PM
2021-05-09 2:26 PM
Voltage and Temperature tend to play a role.
Are you looking for suggestions about checking integrity, using ECC or deep-cycle erasing?
What kind of data are you trying to store/protect?
2021-05-09 2:43 PM
I have two copies of a snes cartridge both use the NOR flash memory STM29W640FT and in that memory the firmware of the cartridge is recorded a copy is saved and I do not use it regularly but if the firmware is erased the cartridge does not work and I want to keep the file always saved in this NOR flash memory
will the files be silently deleted in the future?
2021-05-09 4:58 PM
The flash memory should retain content over many years, if you're losing data something else is likely wrong.
With these type of NOR memories the array could be deep-cycled via Erase, Write All Zeros, Erase, Write New Content
2021-05-09 5:07 PM
I am not losing data and they are recorded in the NOR flash memory M29W640FT 70N6 i doubt How many years does this memory retain data at a temperature of 34ºC?