2005-01-05 04:20 PM
wake up from WFI and keep awake ??
2005-01-05 02:35 AM
mailto:WFI@PRCCU_SMR
again ? Ormailto:WFI@PRCCU_SMR
will keep its value reset automatically after been reset once ? And it only wakes up when an interrupt occurs, then enters WFI again after this interrupt is served. If so, this limits many applications.... I can't say this mcu is good for low power application anymore..... :(2005-01-05 03:31 AM
Hi shinn,
Yes of corse when the device is awakened from WFI mode by an interrupt request it keep awake until next time resetting WFI PRCCU_SMR bit again. The device still runing after this interrupt is served. Best Regards HICH :p2005-01-05 04:20 PM