2020-01-03 09:47 AM
Hello. I'm designing a new board where I use VNI8200XP to control some LEDs and relay loads.
In my case VNI is used in SPI mode (SEL2 pulled high to Vreg), internal DC/DC converter is disabled and Vreg is supplied from on-board +24V/+5V DC/DC Converter.
I'm observing following problem - when the board is powered up or down, some VNI outputs sporadically get high for a short duration (usually 200-400 microseconds).
I investigated the problem and probably found a reason:
At power down, the situation is vice versa - as in my system +5V regulator can't handle as low voltage, as VNI, it shuts off, before VNI becomes inoperational.
I can't allow such sporadic outputs switching at power on/off, so how can I avoid it?
Best regards
Artyom