Using IAP application note with RVDK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-25 4:42 AM
Using IAP application note with RVDK
- Labels:
-
Legacy Products
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-23 2:13 AM
Hi,
I want to try the AN2078 - STR7 In-Application Programming using UART, but the project was created with EWARM and I use RVDK. I searched on the forum but I didn't find a easy solution to convert EWARM projects to RVDK one. Is there a way to do that ? Or must I create a blank RVDK project and fight with the project setting to make it work? Thanks in advance- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-23 7:13 AM
Hi tumnao,
You can just use one example from the existing RVDK Examples library from ST as a template and then just copy/paste the Appli Note main files. It should work smoothly :) Rave. [ This message was edited by: Rave on 23-04-2007 21:48 ]- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-23 10:52 PM
Thanks Rave and ibtiss for your quick replies. I tried different things like using the IAP v2 rvdk project with the IAP v3 sources files, or as Rave suggered a simple exemple in the library, but that didn't do the tricks.
Here is my last attempt step by step : I copied \str71xlibstd\examples\gpio to \str71xlibstd\examples\iap. I added all theses file from the IAP rev3 : 71x_conf.h 7xx_flash.c 7xx_flash.h common.c common.h download.c flash_conf.h flash_map.h main.c ymodem.c ymodem.h I added to project properties *COMPILE=arm/sources/files all the above .c files. I added ibtiss modification to the scat file. At compilation there was theses kind of errors : ''..\..\..\project\include\gpio.h'', line 62: Error: #20: identifier ''inline'' is undefined inline u8 GPIO_BitRead(GPIO_TypeDef *GPIOx, u8 Port_Pin) ^ ''..\..\..\project\include\gpio.h'', line 62: Error: #101: ''u8'' has already been declared in the current scope inline u8 GPIO_BitRead(GPIO_TypeDef *GPIOx, u8 Port_Pin) ^ ''..\..\..\project\include\gpio.h'', line 62: Error: #65: expected a '';'' inline u8 GPIO_BitRead(GPIO_TypeDef *GPIOx, u8 Port_Pin) (..\..\.. refere to the str71xlibstd folder) So I modified 71x_conf.h ''#define inline inline'' line to ''#define inline __inline'' as I saw that in others working 71x_conf.h. I tried to recompile and get : c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armlink --list Listing.txt --entry Reset_Handler --scatter ..\scat.scf --symbols --map DebugRel\ymodem.o DebugRel\download.o DebugRel\common.o DebugRel\7xx_flash.o DebugRel\main.o DebugRel\71x_lib.o DebugRel\retarget.o DebugRel\71x_vect.o DebugRel\71x_init.o -o DebugRel\gpio.axf Error: L6630E: Invalid token start expected number or ( but found F at position 15 on line 34 Error: L6629E: Unmatched parentheses expecting ) but found F at position 15 on line 34 That make me think that I should also modify the entry point in the properties and what about the .s assembly files .... argh In short I am totaly lost with project properties, scatter file and other such low level settings. For my main project, I managed to get it work but I didn't really understant what I done. Is there a good documentation for beginners that I can read before asking stupid question ? :) [ This message was edited by: tumnao on 24-04-2007 11:52 ]- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-24 3:27 AM
Ok, scatter file are more clear to me now (not completly, but more :) )
Now I think my problem come from the 71x_init.s and the 71x_vect.s. In the IAP v3 they are placed under the EWARM folder, and I think this is because they are compiler dependant. Is this correct ? Anyways RVDK complain about syntax like ''MODULE ?program_start'' and ''RSEG IRQ_STACK:DATA(2)''. Anyone know RVDK and EWARM enough to explain me that ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2007-04-25 4:42 AM
Ok I succeded in compiling the IAP v3 with RVDK...
So I had this idea before you send me the .s file ibtiss (Theses file was from the standard STR7 library, right ?) I just had to remove reference to all the IRQ handler has the IAP don't define them. And by the way thank you for the scatter doc, it help me a lot. But all that bring me some new questions : 1) Now the IAP work on my str7 eval board (MB393), but if I want to use it on my own hardware who use a str11f without external ram, am I limited in the size of the application that I can program with the IAP, as I only have 64k of internal ram ? (my application is actually of 140kb in debug) 2) I think I must change the scatter file of my application if I want to program it with the IAP, as the load region won't be the same. Correct ? Anyway thank for the help so far