cancel
Showing results for 
Search instead for 
Did you mean: 

uPsd3354D problem with serial port0

dave1
Associate II
Posted on January 16, 2009 at 18:25

uPsd3354D problem with serial port0

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
dave1
Associate II
Posted on May 17, 2011 at 11:52

Hi,

I have a problem with transmit on the primary serial port on this CPU.

This is the first time I am using a uPSD3354 (have used uPSD3254).

Using the same routines that worked on the 3254, I can send commands on the serial port, but cannot get any output on the TX pin. I have the same prob with more than one prototype. I have checked that the interrupts are occurring and the routine stuffs sbuf, but TXD0 does not change. I can issue a command to change the pin state. (I actually thought that this would not work when not in GP I/O mode)

I have checked all the data and cannot find anything different between the 3254 and 3354 with regard to UART0.

Can anyone help?

Thanks

mattbarlage
Associate II
Posted on May 17, 2011 at 11:52

I am using UART0 with no issues. What are you using to verify data on TxD0?