2026-04-23 12:08 AM - last edited on 2026-04-23 2:18 AM by mƎALLEm
Hello,
I am trying to run Validate on target on a NUCLEO-N657X0-Q board using X-CUBE-AI 10.2.0, but it consistently fails. I would appreciate any guidance.
Environment:
What works:
Problem:
When running Validate on target via STM32CubeMX:
Running the ST.AI c-model (AI RUNNER)...(name=network, mode=TARGET)Proto-buffer driver v2.0 (msg v3.1) (Serial driver v1.0 - COM5:921600)Warning: C-network signature checking is skipped on ST Neural-ART NPULOAD ERROR: STM32 - read timeout 50000msValidation ended
When running stedgeai CLI directly (after manual build via n6_loader.py):
E200(ValidationError): TARGET: Unable to bind the ST.AI runtime with "network" c-modelE801(HwIOError): Invalid firmware - COM5:921600
When running n6_loader.py directly:
Flashing memory xSPI2 -- 48,897.140 kBFlashing memory xSPI2 -- return code ERRORStart operation did not achieve successfully
What I have investigated:
Questions:
Thank you in advance.
2026-05-04 1:58 AM
Hi @qldrh,
Please use STEDGEAI-CUBEAI | Software - STMicroelectronics
We replaced X Cube AI by this new desktop application; X Cube AI status is "not recommended for new design".
You don't have to create a validation application for the Nucleo, we have both the Nucleo and DK.
An update is comming this week allowing you to download 2 applications for every boards:
Have a good day,
Julian