2005-05-13 5:43 AM
2011-05-17 3:06 AM
Hi,
I am working an IAP application for the UPSD3234A. The most of firmware code were based on DK3200 IAP example and I only changed a little bits to disable memory reading founction. The IAP application works well in the most of the time. But something it fails to write data into main flash in the range from 0xFF00 to 0xFFFF. Project info: UPSD 3234A 40MHz Main flash: 0x8000 - 0xFFFF Boot flash: 0x2000 - 0x3FFF Does anyone has similar experience ? Thanks in advance.2011-05-17 3:06 AM