2006-11-02 9:56 PM
2006-11-02 8:17 PM
Hi guys,
I've tried to generate an interrupt from UART TX empty condition, but with no success. My micro is STR11 and I'm working with an evaluation board. Interrupts coming from RX buffer full condition are working pretty well. Someone can help me ? Thanks a lot Giovanni2006-11-02 9:56 PM
Hi guru63,
I tried it as following and it work pretty well. /* EIC peripheral configuration -------------------------------*/ /* Configure the EIC channel interrupt */ EIC_IRQChannelPriorityConfig(UART0_IRQChannel, 1); EIC_IRQChannelConfig(UART0_IRQChannel, ENABLE); EIC_IRQConfig(ENABLE); UART_ItConfig(UART0,UART_TxEmpty, ENABLE); You can send me your code to check it if you still have a problem. Regards, Hich