2007-12-03 4:41 AM
2007-11-07 9:54 PM
Hello all
im having a little bit of trouble with the bspi the clock works perfect and so does sending data but the slave select pin doesnt turn zero to select the device(only one device attached) ive tryed setting it manually but to no avail. please see code belowCode:
void InitaliseQTouch(void) { // P0.0 ''MISO'' // P0.1 ''MOSI'' // P0.2 ''SCLK'' // P0.3 ''SS'' //P2.9 ''DRDY'' //P2.10 ''CHANGE'' GPIO_Config (GPIO0,(1<<1)|(1<<2)|(1<<3), GPIO_AF_PP); // set up port pins. GPIO_Config(GPIO2,(1<<9)|(1<<10),GPIO_IN_TRI_CMOS);//data ready and change pins GPIO_Config(GPIO0,0,GPIO_IN_TRI_CMOS);//MISO //GPIO_BitWrite(GPIO0,3,0x00); BSPI_BSPI0Conf ( ENABLE ); BSPI_Init ( BSPI0 ); BSPI_ClockDividerConfig( BSPI0 ,230 );// this gives a 20 micro wave.10 up 10 down BSPI_Enable ( BSPI0 , ENABLE); BSPI_MasterEnable ( BSPI0 , ENABLE); BSPI_ClkActiveHigh ( BSPI0 , DISABLE);//this should make it idle high BSPI_ClkFEdge ( BSPI0 ,DISABLE); //dont get data on first clock edge BSPI_8bLEn ( BSPI0 , ENABLE); //allow 8 bit words // BSPI_FifoDisable ( BSPI0 ); BSPI_RcFifoDepth ( BSPI0 , 3 ); // 3 Words Recived BSPI_TrFifoDepth ( BSPI0 , 3 ); // 3 Words Transmit } void UseQ(void) { if(GPIO_BitRead(GPIO2, 0x0A)==1)//if change { if(GPIO_BitRead(GPIO2, 0x09)==1)//if data ready { BSPI_BufferSend (BSPI0,Buff1Out,3 );// this should send the words BSPI_BufferReceive(BSPI0,Buff1In ,3 );// put the data recived into my buffer } } }2007-12-03 4:41 AM
Dear noz4r2,
A helpfull basic configuration of BSPI in Master and slave mode is available in thehttp://www.st.com/mcu/download2.php?file=str71xfwlib.zip&info=STR7 Software STR71x&url=http://www.st.com/stonline/products/support/micro/files/str71xfwlib.zip
V4.0. New example for BSPI using interrupt is added as well. Please refer to readme.txt file for the hardware connectivity.