2003-03-06 07:52 PM
TRANSLATING ASSEMBLY CODE FROM HC05 TO ST7
2003-03-05 07:25 PM
Dear Sir,
According to AN1106, it is possible translate the assembly code from Hc05 to ST7 using the ST free utility migr2st7. I would like to know if it is also possible to use the same software in order to traslate from HC08 to ST7. In fact, HC08 is compatible with HC05 core. Thanks in advance for your copperation Gianfranco [ Questo Messaggio è stato Modificato da: dimarcog il 06-03-2003 08:56 ] ________________ Attachments : 1011096740.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I07E&d=%2Fa%2F0X0000000bTh%2F9jVnBEraWRPQGQRTxDQhNtgvdOonc5TA3Vxdh6mRb7k&asPdf=false2003-03-06 07:52 PM
It should work. The best way is to try, but you can also have a quick look on the 2500adcb.h file (installed by the setup) to read all the treated directives.
Good migration!