cancel
Showing results for 
Search instead for 
Did you mean: 

inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s

Posted on March 03, 2003 at 06:43

inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 12, 2003 at 18:26

I have an inDART-ST7/521 kit configured to target a ST72521R9T. At first, I used V1.05 then I recently switched to V1.0.9.

For both versions, I noticed that my ST72521 program was sometime stuck in the crtsx.s startup file (I use Cosmic).

Other times, I have some communication errors using STVD and Data Blaze.

I am sure of my Cosmic code because I have tested it on a ST7 EMU3 emulator. My Indart kit is also brand new.

Any idea to explain these 2 issues ?

Jojo

stephanie
Associate II
Posted on March 03, 2003 at 06:43

When you say you're stucked in the startup file, does that mean stuck on a particular source code line or stucked because of a reset for instance? Check if you're configured in H/W WDG for instance (or place a breakpoint on the first line of the startup to see if the program performs reset).

Do not hesitate also to ask support from Cosmic or Softec!