Skip to main content
NRaha.1
Visitor II
October 21, 2021
Question

STWINKT1B connect to MQTT through 5g wifi

  • October 21, 2021
  • 0 replies
  • 653 views

Hi,

I have a STWINKT1B board which I want to connect to my organization's 5ghz Wi-Fi to be able to send sensor logs to MQTT. To do this what additional hardware do I require (as the WIFI expansion pack for this board only supports 2.4ghz). And is there an example guide / firmware I can follow/use to achieve this?

Thanks

    This topic has been closed for replies.