2021-10-19 5:49 AM
2021-10-20 1:31 AM
Well, JTAG is just the physical layer. In order to be able to program a component with it, the PC software must first be able to address this adapter, and the communication between the PC software and the component must also be correct. So it won't work that way.
Regards
/Peter
2021-10-19 6:47 AM
Welcome, @VReut.1, to the community!
The ST-LINK/V2 can only program STM8 and STM32, not the family of uPSD devices, which have been obsolete for several years.
Regards
/Peter
2021-10-19 6:54 AM
Hi Peter,
thanks for your answer. Do you see any possibility to use a modern USB flash adapter for the uPSD devices? Can I build an adapter?
2021-10-19 7:15 AM
The FlashLINK adapter has a relatively simple structure, but unfortunately there is no longer any documentation on what the protocol looks like on the parallel port. In this respect one would have to analyze this protocol again and then develop a programming adapter with USB.
Is it really worth it or isn't it better to dig up an old PC with a parallel port to program with the FL-101?
Regards
/Peter
2021-10-20 12:26 AM
I am not super familiar with JTAG, but can't I just use TMS,TCK, TDI, TDO pins of the ST-Link/V2 and connect them to the uPSD or is the protocol totally different?
2021-10-20 1:31 AM
Well, JTAG is just the physical layer. In order to be able to program a component with it, the PC software must first be able to address this adapter, and the communication between the PC software and the component must also be correct. So it won't work that way.
Regards
/Peter
2021-10-20 1:57 AM
Ok, understood. Thanks, Peter.