2007-12-05 8:49 PM
2007-12-05 1:58 AM
Hallo,
I want to debug the provided software for PMSM motors. If I tried to execute ''rebuild all'' in IAR Embedded Worckbench it shows me some errors: Error[109]: Expression is too complex K:\projekt\STR750_servo\IAR_infos\foc_pmsm\FOC_PMSM_SR_v1.1\IAR\config\75x_init.s 250 Error while running Assembler 75x_it.c 75x_pwm.c 75x_tb.c 75x_vect.s Error[40]: Bad instruction K:\projekt\STR750_servo\IAR_infos\foc_pmsm\FOC_PMSM_SR_v1.1\IAR\config\75x_vect.s 21 Error while running Assembler MC_Display.c after i tried to debug software, the demo software on the eval.board dosn't work anymore. and I cold not to reprogram this. It shows me: Bad JTAG communication: Write to IR: Expected 0x1, got 0x7(TAP Command:2)@ Off 0x5. How can i solve this problem?2007-12-05 8:49 PM
Hi,
It seems that you are using the new version of EWARM 5.10A. And in this case you need to update the assembler files and use the new linker file(*.icf). Those files are available under: ''C:\Program Files\IAR Systems\Embedded Workbench 5.0 \ARM\examples\ST\STR75x\STR75xLibrary'' Rgds, Zouhair