cancel
Showing results for 
Search instead for 
Did you mean: 

STHV748 Capacitor size

nstc001
Associate
Posted on September 01, 2014 at 09:34

What is the range of capacitor sizes recommended to AC couple the substrate (exposed paddle) to ground? A 0.22uF is shown in the Application Note AN3961. Is there a limit on maximum size? Can the substrate be connected to the most negative HV supply? 

#sthv748 #ultrasound
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ricotti.giulio
Associate
Posted on September 17, 2014 at 08:49

Dear Reel,

your question is clear, yes, the substrate, througth the exposed pad, it si preferable to filter it by a HV capacitor connected to clean GND, in principle there is no limit to the maximum value of this capacitor.

It can also be connected to HVM0.

Best Regards

Giulio Ricotti