Skip to main content
econfalonieri
Associate III
September 12, 2003
Question

ST92T141 programming specifications

Posted on September 12, 2003 at 06:45

ST92T141 programming specifications

This topic has been closed for replies.

2 replies

vincent239955_stm1_st
Visitor II
May 17, 2011
Posted on May 17, 2011 at 11:34

Hello

One can do ISP JTAG with ST92E141 EPB, thanks to the W1 connector (cf pin-out here below).

Beware that the inputs OSCIN, RESET et VPP, managed by the EPB, must be deconnected when programming; Clearly this is a limitation of this approach (together with the JTAG high pin count).

Best regards,

VO

---

W1 is a 16-pin connector (2.54mm pitch = HE10).

TMS 1 - 2 OSCIN

TCK 3 - 4 RESETn

TDI 5 - 6 TEST0

TRST 7 - 8 NC

TDO 9 -10 NC

NC 11-12 NC

NC 13-14 VPP

GND 15-16 GND

NC = Not Connected

TMS = P5.3

TCK = P5.4

TDI = P5.2

TRST = P5.5

TDO = P5.0

TEST0 = P5.7

[ This message was edited by: vonde on 12-09-2003 10:18 ]
econfalonieri
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:34

Hello,

FAE from Italy here...

A customer using ST92T141 is asking us some information on how to perform an in circuit programming on this OTP microcontroller in such a way to optimize board manufacturing. Which pins are involved? Is there some documentation about it?

Best Regards

E.C.