2013-07-30 3:08 AM
Hi
I have a new build PCB with a ST7Flite29 fitted, I cant program the device, I have had to run an external clock signal to Clk In (PB4), the programmer is now reporting ''Write Protected'', how do I get this back, the ERASE device is greyed out on the STVP programmer Regards, Brian2013-08-12 5:39 AM
Hello,
Normally, a brand new ST7 should not be write protected. Anyway, in STVP, read option bytes and then just change the option bit FMP_W ''WRITE protection'' to OFF and reprogram the options bytes. Then, you can reprogram the program memory.(If the FMP_R is OFF too). Rgds, Laurent