2007-03-12 4:12 AM
2007-03-08 5:47 AM
Hi,
I can not find my mistake. I want to clear the Int. flash & it does not work. May somebody have a look in my code? The code is executed from RAM, it's ok. Thanks a lot. Gabi mkC ST10F269 [ This message was edited by: gaby_bradu on 08-03-2007 19:19 ] :o Sometimes there are very simple errors. It Works. [ This message was edited by: gaby_bradu on 09-03-2007 09:59 ] ________________ Attachments : erase.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0M4&d=%2Fa%2F0X0000000bXp%2FYnJsO25iXiCbb1JXMY8xvkyBJyVs3rxbsYiySUwSbc8&asPdf=false2007-03-09 2:04 AM
Thanks Neila,
ROMEN = 1 ROMS = 0 R8&9 - (0/0; 0/4; 0/6; 1/0; 2/0...) It works for the Bank 0 R8&R9 = 0. (deletes my software :)) My controler goes through reset if I call the function below, on this point: MOV [R5],R7 :( Is something wrong configured? Thanks a lot, Gabi. PFlash_RP PROC NEAR MOV R1, #2H ; The second page MOV R5, #02A54H ; For the 1st & 3rd write MOV R6, #015A8H ; For the 2nd write MOV R2, #0A8H ; MOV R3, #54H ; MOV R7, #90H ; EXTS R1, #4 MOV [R5],R2 ; 1st command MOV [R6],R3 ; 2nd command MOV [R5],R7 ; 3rd command MOV R4,[R1] ; 4th command RET PFlash_RP ENDP [ This message was edited by: gaby_bradu on 09-03-2007 15:36 ] [ This message was edited by: gaby_bradu on 09-03-2007 15:45 ]2007-03-11 11:30 PM
Hi Neila,
Thank you for your help. The WDTCON register I did not read. The following hardware traps are analysed in my software & no one comes: void NMI_trap (void) interrupt 0x02{...trap_cause = TFR;...} void STKOF_trap (void) interrupt 0x04{...trap_cause = TFR;...} void STKUF_trap (void) interrupt 0x06{...trap_cause = TFR;...} void Class_B_trap (void) interrupt 0x0A{...trap_cause = TFR;...} But I'll check all this points once more & I'll be back soon. Thanks a lot. Gaby. 8-)2007-03-12 2:36 AM
So I'm back, I did some tests......
it was the watchdog, after the RP function and it restarts I read 0x06. But it can not be because I service the WD. I disabled the WD DISWDT EINIT and now it hangs-up. :( I did a small change in the RP procedure and it never returns: EXTS R1, #3 MOV [R5],R2 ; 1st command MOV [R6],R3 ; 2nd command MOV [R5],R7 ; 3rd command RET MOV R4,[R1] ; 4th command The generated code from RP function is: :10300000E021E6F5542AE6F6A815E6F2A800E6F374 :103010005400E6F79000DC21B825B836B875CB002F :04302000A841CB00F8 After the instruction B875 it hangs-up. Thanks, Gaby. P.S. I copy this code on address 0xC000 (or 0xE000), it's free. int (*PFlash_RPP)(void); ..... PFlash_RPP = (void *)0xC000; xmemcpy((ubyte huge *)PFlash_RPP, (ubyte huge *)PFlash_RP, 80); ..... tst = PFlash_RPP(); [ This message was edited by: gaby_bradu on 12-03-2007 15:55 ]2007-03-12 3:46 AM
Hi Neila,
I send the sources on your e-mail (neila_kraiem@yahoo.fr). The rest you can see from the code. Thanks, Gaby.2007-03-12 4:12 AM
My e-mail is:
mailto:gaby_bradu@yahoo.com
Gaby.