cancel
Showing results for 
Search instead for 
Did you mean: 

st10f269 code Temporary Unprotection

y_gudekar
Associate II
Posted on February 22, 2006 at 09:47

st10f269 code Temporary Unprotection

2 REPLIES 2
y_gudekar
Associate II
Posted on February 22, 2006 at 08:59

hi,

Once Code Protection Set in St10F269,then what is the exact sequence to reprogram it using St10 Flasher and Code Temporary Unprotection command?

najoua
Associate II
Posted on February 22, 2006 at 09:47

Hello,

Once Code Protection is set in the ST10F269, it is no longer possible to use the ST10Flasher tool ,as it is, to reprogram the flash.

In order to be able to use the ST10Flasher tool to reprogram the flash after being protected, we should update the monitor source ... and the Code Temporary Unprotection command must be located in an unused location (that will never be erased) in the flash to be called when needed.

Regards,

Najoua.

[ This message was edited by: Najoua on 22-02-2006 15:27 ]