cancel
Showing results for 
Search instead for 
Did you mean: 

IAP driver for IAR compiler

anil23
Associate II
Posted on February 22, 2006 at 12:09

IAP driver for IAR compiler

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
anil23
Associate II
Posted on December 08, 2005 at 16:37

Hi,

I was looking for some sample code if someone had the IAP driver running on the IAR compiler

Thanks

anil23
Associate II
Posted on December 12, 2005 at 14:19

Thanks a lot,

I have taken the task of porting the IAP driver on the USB. Lets see how successful i would be!

anil23
Associate II
Posted on February 15, 2006 at 12:04

Hi Zouh,

I realized that the IAP driver files need to run from the RAM. But the linker file in the example doesn’t load the files to RAM. When I try to execute your code the file download is performed fine. But, when I try to program…it gives me an error that “There is no file to be programmed….� And after couple of seconds the terminal windows quits.

Please update me with the project/linker files of IAP driver for IAR.

Regards,

[ This message was edited by: iamanil on 15-02-2006 17:06 ]

anil23
Associate II
Posted on February 15, 2006 at 13:54

Hi Zouhair,

Thanks for all your help.I followed your instructions and performed them on my STR710 board.

I can download the file now. But its not programming the internal flash(when i press 2 on the hyperterminal). It returns a ''E'' on the hyperterminal and returns to Main_Menu().

Please find attached the updated project and the file I'm downloading.

Also, the LED20 on the board is turning red after i download the program.

Regards,

[ This message was edited by: iamanil on 15-02-2006 18:26 ]

________________

Attachments :

IAP-IAR_v1.1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtHN&d=%2Fa%2F0X0000000aL1%2FXTMpC8ezNSUHj0dASIBccUWecFFRYpIoPJmiUrwaa38&asPdf=false

STR710-Eval.a79 : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtHX&d=%2Fa%2F0X0000000aL2%2FkiCz3bQEEa_tMTCxS3uLDJZFZ4jYWU4aoGkT.G7skII&asPdf=false
anil23
Associate II
Posted on February 15, 2006 at 15:42

Hi Zouh,

Yes! I did. I'm sorry for not mentioning that in my prevous message.

I did press 1 for download..it downloads the file fine and displays the file information (size and name of the file) on the terminal window.

Then, when i try to press 2, I get the message ''E'' and the program jumps back to Main_Menu();

If you could run the attached project and download the file attached fine on your MB 393 board . Please let me know.

Thanks,

anil23
Associate II
Posted on February 16, 2006 at 16:39

Thanks Zouhair,

It seems to work now...I will let you know if i come across any problems.

Regards,

anil23
Associate II
Posted on February 17, 2006 at 02:37

Hi Zouh,

Please help me understand the process for generating the binary file using IAR. Did you generate it under Project->Options->Linker->Extra Output->Generate Extra Output with output format as raw binary?

Please let me know.

Regards,

anil23
Associate II
Posted on February 17, 2006 at 15:44

Hi Zouh,

I followed your instructions to generate a binary file from the IAR demo board example. I got a programming error while downloading to the flash.

Please find attached the project for your reference.

Regards,

________________

Attachments :

STR710-EVAL.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtHh&d=%2Fa%2F0X0000000aL3%2F0HRE2Me5_8rgIi44gG5bHKGAK5ffyW_omjZ3RscQEhQ&asPdf=false
anil23
Associate II
Posted on February 21, 2006 at 20:34

Hi Zouh,

Thanks for the updated project. I have made a step forward in my attempts to make IAP work through the USB. It's working with the bin file for the example.

Regards,