2006-03-13 8:59 PM
some questions about the 71xboot-R10 in the Package of uClinux for STR71x
2006-03-12 5:57 PM
hi,all
i have designed a board with str710 boot in flash mode,and i want to use the 71xboot-R10 in the Package of uClinux for STR71x,and i have write a scat file as this: FLASH_MODE 0x40000000 0x40000 { FLASH 0x40000000 0x40000 { 71x_vect.o (Vect, +First) 71x_init.o (Init) * (+RO) } RAM 0x20000000 0x10000 { * (+RW) * (+ZI) } } but it could not execute right after i loaded the image in the flash(0x40000000) :o2006-03-13 12:08 PM
thanks Zouhair,
i have see the pdf document,but there are some different things on my board: (1)clk is 11.0592M but not 16M (2)sram size is 1M (3)booting flash mode but not externel memory (4)i use uVision3 instead of ADS so i have to modify the 71xboot-r10 in order to fit my board. and i think after modifing the 71xboot-r10 i should link that newly in order to booting form cpu flash. is that right?2006-03-13 8:59 PM
i have found the solution,
i found that in the 71x_boot,uart.c about the type define of BaudRate using ''u32'' made the mistake in rs232.