2004-11-17 1:14 AM
SD Card in SPI Mode (byte alignment problem)
2004-11-14 11:04 PM
Is there anyone who you help me with a problem I'm having writing a proprietary software interface to an SD card.
I'm trying to read/write the a SD card in SPI mode, but I keep getting byte misalignment in the responses to SPI commands. For example, if I send CMD0 (40 00 00 00 00 95) to put the card into SPI mode, I sometimes get back 0xff 0x1 0xff, which is correct, but sometime I get 0xff 0xC0 0x7f 0xff, and other spuriously misaligned responses. The alignment also seems to vary each time the device is selected (/CS). And sometimes I find that I can't select SPI-bus operation!!! I'd be grateful of any help. Regards2004-11-17 1:14 AM
Many thanks to anyone who's looked at this and given it a second thought - but (I think) I've managed to fix my problem. And for anyone interested, you need to set CPOL = 0 and CPHA = 0, and to continually send the MMC_GO_IDLE_STATE command (after sending 4 sets of 0xFFs) until the SD card is fully in SPI mode with a response of 0x1. After this you're ready to go, and can poll the MMC_GO_IDLE_STATE status busy flag.