2003-06-23 11:01 PM
Running code from GCC using STPC bootloader in real mode
2003-06-19 12:35 AM
Chaps,
I've got a problem which I cant work out. I'm using an STPC elite evaluation kit and booting the CPU using the STPC bootloader. I've written some code using GCC, setup as a cross compiler in RH7.2 for i486-coff. I'm booting in real mode, and copy/executing from 10000h. I'm using a 128K flash, and copying all of the top 64K to 10000h. The code i've written is below, but in low-level as this is what i understand. The problem is the code gets as far as a call and stops. Well i think it's the calls that are stopping it, but i'm a little unsure. When booting the system, I get all the normall post codes from the boot loader. Then the post code display should show 'CC', then 'DD', then 'BB'. Although I'm only getting as far as 'DD'. 'BB' is output by section __main which is called by section main. After main is called, only ebp/esp get changed and __main is called. I can't understand why 'BB' is never displayed, as changing esp/ebp should not effect the call (only the stack). Any help? PS the code is in AT&T standard format (not masm) a.out: file format coff-i386 Disassembly of section .text: 00010000 : 10000: 31 c0 xor %eax,%eax 10002: 8c c8 mov %cs,%eax 10004: 8e d8 mov %eax,%ds 10006: 8e c0 mov %eax,%es 10008: b0 cc mov $0xcc,%al 1000a: e6 80 out %al,$0x80 1000c: bc 04 00 00 00 mov $0x4,%esp 10011: b8 08 12 00 00 mov $0x1208,%eax 10016: 8e d0 mov %eax,%ss 10018: b0 dd mov $0xdd,%al 1001a: e6 80 out %al,$0x80 1001c: e8 07 00 00 00 call 10028 10021: 8d b4 26 00 00 00 00 lea 0x0(%esi,1),%esi 00010028 : 10028: 55 push %ebp 10029: 89 e5 mov %esp,%ebp 1002b: 83 ec 08 sub $0x8,%esp 1002e: 83 e4 f0 and $0xfffffff0,%esp 10031: b8 00 00 00 00 mov $0x0,%eax 10036: 29 c4 sub %eax,%esp 10038: e8 3e 00 00 00 call 1007b 1003d: b0 aa mov $0xaa,%al 1003f: e6 80 out %al,$0x80 10041: c7 45 fc 00 00 00 00 movl $0x0,0xfffffffc(%ebp) 10048: 81 7d fc fd ff ff 7f cmpl $0x7ffffffd,0xfffffffc(%ebp) 1004f: 7e 02 jle 10053 10051: eb 0b jmp 1005e 10053: b0 11 mov $0x11,%al 10055: e6 80 out %al,$0x80 10057: 8d 45 fc lea 0xfffffffc(%ebp),%eax 1005a: ff 00 incl (%eax) 1005c: eb ea jmp 10048 1005e: c7 45 fc 00 00 00 00 movl $0x0,0xfffffffc(%ebp) 10065: 81 7d fc fd ff ff 7f cmpl $0x7ffffffd,0xfffffffc(%ebp) 1006c: 7e 02 jle 10070 1006e: eb d1 jmp 10041 10070: b0 22 mov $0x22,%al 10072: e6 80 out %al,$0x80 10074: 8d 45 fc lea 0xfffffffc(%ebp),%eax 10077: ff 00 incl (%eax) 10079: eb ea jmp 10065 0001007b : 1007b: 55 push %ebp 1007c: 89 e5 mov %esp,%ebp 1007e: b0 bb mov $0xbb,%al 10080: e6 80 out %al,$0x80 10082: 5d pop %ebp 10083: c3 ret Disassembly of section .data:2003-06-19 4:35 AM
MurF,
When you start the loader in real mode, the data segments DS and ES are initialized in the GDT in ''flat mode'' and can access the whole memory. It is not the case for the code segment CS which have got the standard real mode limitation of 16 bits for the offset. This means your jump to 10028 is going to perform a jump to 0028 and have to be replace by a far jump to 1000:0028 (CS=1000 then a jump to 002 . To be honest, it will be quite difficult to use gcc in real mode. The compiler have been designed for 32bits protected mode. You will probably also have to manually switch your segment from 16bits to 32bits in the GDT. I highly suggest you to use the example of secondary loader you get from the STPC Development Kit available on this web-site. The examples of loader present in this kit are downloading and executing a WinCE image or a Linux kernel but you can easily replace by your own code. It is also written in C language for gcc Farfalla2003-06-23 11:01 PM
Ta. Lovely. Thanks. Nigel.