2008-05-09 11:12 AM
Running Bootloader from Bank1 and Switch to Bank0 Application
2011-05-17 12:53 AM
I did develop a bootloader for ARM9 to run from Bank1 and later switch to bank0. When I ran the same bootloader from Bank0 I could debug and test its working.
But when I changed the program to run from Bank1 (in IAR 5.10 Release Mode) its not working. Using JlinkSTR91x.exe I am changing boot bank to 1 by running the command the ''setb 1''. Then trying to load the program to flash from IAR (Release Mode). Then I tried to cycle power the ST ARM9 MCU but my program doesn't seem working. Any ideas quickly??2011-05-17 12:53 AM
It will only work with revH silicon.
see the errata for more details. Cheers sjo