2004-04-20 12:23 PM
2003-06-09 11:52 PM
Is there somebody using a RTOS in his own application ?
What RTOS ? Thanks, Patrik2003-06-10 10:26 PM
RTOS means Real TIme Operating System. Some of ST third-parties develop some (ex: CMX, ...). You can have information on their Internet site.
2003-06-10 10:52 PM
I know what does RTOS mean...
I made the question because I need REAL data about the requirements of RAM and ROM. I want to know if an RTOS like CMXTiny+ or uC/OS-II is usable in my low-cost system (384 bytes RAM, 8K Flash)...and wich of them you suggest. I need only the multi task management feature. Thanks, Patrik2003-06-10 10:58 PM
Have a look at embOS from Segger
http://www.segger.com They have also given the resource and performance data for ST7 on following link http://www.segger.com/cpust7_cosmic.htm Regards, PraveenG2003-06-10 11:16 PM
That's what I was looking for !
Thank you very much! Patrik2003-06-16 2:31 AM
I found some minimal RTOS:
-http://www.nilsenelektronikk.no/
(Nilsen Elektronikk as ) -http://xmk.sourceforge.net/docs/
- eXtreme Minimal Kernel -http://liquorice.sourceforge.net/
-http://www.nbb.cornell.edu/neurobio/land/STUDENTPROJ/1999to2000/greenblatt/index.html
- they aren't ported to ST7 yet and are free. Another possibility is uC/OS-II that is available for ST7. Patrik2004-04-20 12:23 PM
I have written a small multitasking engine for the Cosmic C compiler.
You can have up to 254 tasks, (well, not in reality as you are limited by RAm available). I have implemented mutexes and basic semaphores. I have attached it.... Good Luck !! ________________ Attachments : romsched_0_1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Ac&d=%2Fa%2F0X0000000bUh%2FSaJj.NsKXefHtxkcylVoxKG3rFMsqbHdwR0gCYxqb8w&asPdf=false