2008-03-21 6:08 AM
2011-05-17 12:50 AM
I developed a network bootloader using uIP. The bootloader resides in Bank 1, it starts then if it finds a valid application in BB0 runs it.
I need to be able to restart the STR9 from within the application in BB0. Is there any reset instruction?2011-05-17 12:50 AM
Dear dibacco,
There is no reset instruction, but you can make a Watchdog end of count Condition (WDG Reset) which is a system reset. By the way, there is an IAP over Ethernet “AN2675�? already available through this link: http://www.st.com/mcu/familiesdocs-101.html Kind regards, Eris.