2025-03-24 5:30 PM
Dear forum
I need to update a board that uses BMO055 9 axis IMU and I need to know what is the preferred ST solution that best fit this obsoleted part.
I need the 3 axis gyro + 3axis accelerometer + 3 axis magnetometer
If there is a single chip solution its okay, but a dual chip solution can work as well.
Thanks in advance
Ignacio
Solved! Go to Solution.
2025-03-26 12:23 PM
Well, NanoEdge AI Studio is free of charge for users of STM32. Users of MCUs with Cortex-M from other manufacturers can purchase a licence by contacting their local distributor or the nearest sales office of STMicroelectronics. As ESP32 is not based on Cortex-M, this option is not available there.
Regards
/Peter
2025-03-25 1:31 AM
You could check these alternatives:
Hope that helps?
Good luck!
/Peter
2025-03-25 5:11 AM
Hey Peter!
Thank you for your suggestion. Now What are the differences between the ISM330 series IMUs and the LSM6 series IMUs?
And, inside the ISM330 suggested sensors, do they require further programming/firmware uploads in order to work properly?
Thanks in advance
Ignacio
2025-03-25 5:31 AM
The MEMS whose order designation begins with the letter "X" are so-called consumer devices whose availability period depends on the major customers who use them in their products. As soon as demand falls (usually between 3 and 8 years after the sensor is released), they are discontinued.
An "I", on the other hand, stands for "Industrial" and guarantees availability for 10 years from the start of production.
All MEMS must be configured, some require some programming, but this is described in the data sheets and application notes of the devices.
2025-03-25 5:41 AM
Hello Peter
Thank you for the guidance in part number designation!
My question was aimed to know if the suggested parts required some code for it's internal processor to be uploaded previous to the device operation.
Best
Ignacio
2025-03-25 6:47 PM
Peter
I have a doubt with the ISM330IS and NanoEdge AI studio,
The page says that the libraries are optimized for running on a STM32 chip
but our system uses ESP32 module as processor. Is it mandatory to use an STM32
for the IPU code?
Best
Ignacio
2025-03-26 12:23 PM
Well, NanoEdge AI Studio is free of charge for users of STM32. Users of MCUs with Cortex-M from other manufacturers can purchase a licence by contacting their local distributor or the nearest sales office of STMicroelectronics. As ESP32 is not based on Cortex-M, this option is not available there.
Regards
/Peter