User Activity

Dear forumI need to update a board that uses BMO055 9 axis IMU and I need to know what is the preferred ST solution that best fit this obsoleted part.I need the 3 axis gyro + 3axis accelerometer + 3 axis magnetometerIf there is a single chip solution...
DEar forum I'm designing a system to use a quad spi memory for log purposes. And I see that the L412R8I only features qspi bank 1 on AF10Bank 0 is missingIs it okay? I'd only use it by indirect access, because the memory is to be read and written Are...
Dear allI'm starting a design with the  STM32L412R8I (or  maybe STM32L412RBI6) and I cannot find the VBUS dedicated pin in the datasheet nor in the manual. In this design the USB will be always device (no OTG)Is it enough to have VDDUSB powered to de...