2006-07-21 5:12 AM
2011-05-17 2:50 AM
After looking of the uPSD34xx - USB Interface documentation, I need help with sample source codes other explanations on ''Reading and Writing FIFOs'' (CPU side =mcu34xx, with XDATA,USEL/UCON/USIZE,USCV/USCI and defining endpoint1_IN, endpoint3_OUT(each 64 bytes max), using DK3400 and Keil). I am newbie and would like to try an application later. The idea is to read and write bytes to/from FIFOs ep1_IN and ep3_OUT...which functions i am going to use? By setting the Visible-bit(UCTL) do i first mapped the UBASE-Address in XDATA space? USEL for selecting my endpoint with direction...and how continuing?
waiting for your help/answer. Thanks, Val