2006-07-24 3:02 AM
2011-05-17 2:50 AM
3V/5V incompatibility at port P1 with (all?) the turbo series. The following phenomenon
has been observed with UPS3354D and UPSD3334D: if a digital input at P1 is driven high (to VDD = 5V) by an external device, all analog inputs are corrupted (pulled high through some internal resistors). This can be easily seen at the DK3300-ELCD demo board: 1 - Make sure that a jumper is installed at ADC7 (header JP14). 2 - Use the ''Banking'' demo program from the CD (or the site). 3 - Run the PWM/ADC test. Observe the ADC reading going from 3FFH down to near 0. 4 - Using clips, connect a 3K resistor between ADC0 (JP14) and 5V at the M41ST87 connector. 5 - Now the ADC reading cannot go below 100H. The non-turbo UPSD3254D has no problem in the same condition. I sent a note to STmicro support more than one week ago, and I got no answer. Can somebody confirm this issue. Mr Moderator, can I have your opinion? Daniel