2006-05-09 10:51 PM
2006-05-09 9:16 PM
Hello Everyone,
I have a question regarding the RAM Area of the ST72F521R9T microcontroller. its RAM range is from 0x200 to 0x87F. Inorder to distinguish from the bootloader and the application i have preserved a location in the RAM which will not be initialised to 0 at the startup ,so that based on that location the bootloader can decide to go to appln or soft upload mode. i used values 0x00 for application and 0xFF for download mode, but now on some boards i saw that the application was not starting ,upon debugging i found that in that board as soon as the power was switched off and powered on the location which i had used to distinguish between application mode and upload mode becomes by default 0xFF every time i put off the power and put it on again, can you help me to solve this problem also on my board i dont have any I2C EEPROM so that i could had used that for storing the variable. waiting for the reply, Thanks Vikram S.M.2006-05-09 10:51 PM
At a cold reset the ram value is undefined, so your approach will not work.
Why not use a crc checksum which you write after programming the appli flash. If the checksum is ok run appli if not run your bootloader. This is the common method used. Regards sjo