2005-05-03 4:37 AM
2005-05-02 11:32 PM
Hello
I've seen that between the RTCXTI et RTCXTO pins, we have to place a 32KHz quartz for the realtime clock. If if generate this clock by a FPGA, is it possible to connect this signal on the RTCXTI pin, and to put the RTCXTO one on the ground? If not, is there a solution? Thx Dam :D2005-05-03 4:37 AM
Hello Dam,
In the STR71x Reference Manual (Page 63/345) it's indicated that you can stopped or bypassed the 32-KHz oscillator , featuring zero power consumption and allowing an external reference clock to feed the Real Time Clock, or a Backup clock source to the whole system. So I think that your idea is actable. Best regards, Hich ;) [ This message was edited by: Hich on 03-05-2005 17:27 ]