Posted on June 14, 2005 at 12:26I don't use RDVK. We have choosen WinIdea IDE with IAR compilator. In my memory windows, icn't write data at the 0x62000000 address... Regards Dam
Posted on June 14, 2005 at 12:11hello; My code is executed in the internal Flash mapped at 0x0. The boot mode is: SW15 = 0 SW14 = X SW13 = X I use the EMI to enter data in the external ram... After, it will be used to dialog with a FPGA. Is there ...
Posted on June 14, 2005 at 08:04I've wrote those lines in my program: So i initialize the bank 1, witch is conected to the external SRAM, and then, i write the number 0x55 into it, and read it... Then, in my program, i send the ''data'' on the RS232...