cancel
Showing results for 
Search instead for 
Did you mean: 

PSD Express, relation of files and tools, building from command line

mviotto
Associate II
Posted on November 12, 2003 at 16:49

PSD Express, relation of files and tools, building from command line

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
mviotto
Associate II
Posted on May 17, 2011 at 11:56

PSDSoft is a good tool to get a result within short time but I am a bit confused about the type of files which are produced. Can somebody inform me about which files are the input to which tools and what output files are produced?

I store every source file of a project in a revision control system and it would be nice to know which files are ''original'' data and which are generated or just temporary data.

There are a lot of ''exe''-files in the PSD directory. Is it possible to have the complete project built up from the commandline?

Michael