cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with ST7MDT2-EMU2B and ST7 visual develop. SW

pmd
Associate II
Posted on December 20, 2005 at 06:31

Problems with ST7MDT2-EMU2B and ST7 visual develop. SW

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
pmd
Associate II
Posted on December 19, 2005 at 11:23

Hi.

I have 2 problems.

1. I have a ST7MDT2-EMU2B emulator and I would like to have this emulator to work on windows XP.

I can't connect to the device? I'm aware that the datasheet says that I should run the device on a 95/98/NT machine. Has ST made a LPT driver for 2000/XP?

2. I have a SW that has been written in CodeWarrior IDE, and I would like to have this code running in the ST7 visual develop. 3.00 SW.

I choose the ''Metrowerks'' under ''Linker'' and then I add the *.c and *.h files to the project.

When I compile / build the project, it comes up with all kinds of errors... The code can be compiled under the CodeWarrior IDE with NO errors at all. How can I make the ST7 visual develop. SW compile the code the right way and get to working with the debugger (ST7MDT2-EMU2B)?

What am I doing wrong?

Thanks in advance.

Regards.

Peter

Denmark

laurent239955_stm1
Associate II
Posted on December 20, 2005 at 06:31

Hi,

1. You should have an old datasheet, because the EMU2B works now with XP and W2000

2. Did you select MW when you create your workspace in the toolchain text box ? Did you select your PRM or keep the default one ?

''All kind of errors'' is not very helpful to help you. If you can give us more clues!

BR

laurent

[ This message was edited by: laubey on 20-12-2005 15:16 ]