2003-10-23 3:09 AM
Problem with ST7LITE05 Watchdog Timer
2003-10-20 3:11 AM
1) I configured the MCU for hardware WDT and no reset on Halt
2) Before executing the Halt instruction I wrote this code: bset LTCSR,#0; Clear Watchdog Timer halt 3) After reset vector fetch I wrote this code: .main bset LTCSR,#0; Clear Watchdog Timer 4) When the MCU is stucked and the WDT resets it I can see in the scope in the external reset pin(3) the reset pulse of about 30 us and then it is released for about 45 us. I suppose it belongs to the internal reset 256 Tcpu + the Vector fetch time and then the low reset pulse again. 5) The MCU fails to wake up in normal mode because the WDT is not fully cleared and I don't know what else I have to do in order to assure the WDT won't reset the MCU immediately after RESET sequence. bset LTCSR,#0; Clear Watchdog Timer seems not to be enough for this purpose even before entering Halt mode and after Reset vector fetch Thanks Claudio2003-10-22 5:59 AM
Did you clear the WDGRF Flag after the Watchdog Reset.
If you have not cleared it, this could be the reason why the microcontroller is immediately reset again. I hope this helps.2003-10-23 3:09 AM
The only thing required is to refresh the watchdog counter before entering into the halt mode; So make sure it is done