2007-06-14 4:01 AM
2007-06-14 4:01 AM
I am planning to use the HOLD/HLDA bus sharing mode on the ST10F269 so that another CPU can write into XRAM on the ST10's bus.
I use ST10F269 Microcontroller Slave mode The ST10F269 works with the program in the inside flash Signals pins: ST10F269(EA=1) ST10F269(HLDA=1) CPUmaster(CS) >>> ST10F269(Hold) CPUmaster(RD) >>> ST10F269(RD) CPUmaster(WR) >>> ST10F269(WR) CPUmaster(16bit data) >>> ST10F269(16bit data) CPUmaster(address) >>> ST10F269(address) Problem: if the slave(ST10F269) read xram when it enters hold mode and the master write in the xram, the data they are introduced an one wrong address