2004-07-21 2:12 AM
2004-07-19 4:03 PM
OSCRANGE of option byte is meaningful only when resonator is used?
if 8MHz is used, then which setting is prefered? HS:8-16MHz or MS:4-8MHz?2004-07-19 11:52 PM
If 8MHz is used then you should go for MS:4-8MHz.
2004-07-20 3:11 AM
OSCRANGE is necessary for two reasons:
1. to select the suitable source about the oscillation circuitery when you are using a resonator 2. to set the nominal frequency on other conditions. Concerning your question you can select HS:8-16MHz or MS:4-8MHz. Luca [ This message was edited by: Luca_Defend on 20-07-2004 15:42 ]2004-07-20 8:55 PM
Hi Luca,
But isn't it true that since the oscillator driving current is less when you select the option MS:4-8MHz instead of HS:8-16MHz. In that case though you can use both it is preferable to use MS:4-8MHz. Thanks Ansh[ This message was edited by: Ansh on 21-07-2004 09:26 ]2004-07-21 2:12 AM
It is true!
I share your opinion Luca [ This message was edited by: Luca_Defend on 21-07-2004 14:46 ]