cancel
Showing results for 
Search instead for 
Did you mean: 

Original Short Range RFID DemoKit firmware on upsd3422ev does not compile

fabrice239955
Associate II
Posted on May 30, 2007 at 13:28

Original Short Range RFID DemoKit firmware on upsd3422ev does not compile

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fabrice239955
Associate II
Posted on May 17, 2011 at 11:51

Hello, I got the demokit with upsd3422ev, and the code (firmware) supposed to be working on the processor.

Teh 1st thing I did was to launch the Build of the code and the problem is that the code (without updating anything) is failling

under Keil Build process.

I got this error message:

<

assembling STARTUP34.A51...

compiling appli.c...

compiling autonomous.c...

AUTONOMOUS.C (934): error C249: 'DATA' : SEGMENT TOO LARGE

compiler Encoder.c...

...

>>

Does someone has any idea about what is failling?

Is there any update of this code somewhere?

I attached the screenshot of this error

Thank you in advance! :)

fabrice

:p

[ This message was edited by: tiofabby on 30-05-2007 17:14 ]