cancel
Showing results for 
Search instead for 
Did you mean: 

RLink incompatible to PSDSoftExpress

fechner
Associate II
Posted on June 15, 2007 at 06:09

RLink incompatible to PSDSoftExpress

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
fechner
Associate II
Posted on May 17, 2011 at 11:51

Hello,

some more info:

I can program the PSD successfully once. If I remove the RLINK

from the USB port and connect it to a differt USB port, I can

program the PSD a second time. If I switch back to the first

USB port, it work a third time.

So this is a working workaround, but what is the reason for this

behavior and how to fix it?

Regards:

Uwe Fechner

fechner
Associate II
Posted on May 17, 2011 at 11:51

Hello,

if I start WinFLink I get the message:

Error communication (0304)

Hint: This version of the software only handles RLink with

firmware version up to 0.0.255 .

This does not always happen, but always after I programmed the

flash of the PSD813F1-U the first time.

Any idea?

Can I use a newer version of PSDSoftExpress or downgrade the firmware

of RLINK?

I am using PSDSoftExpress 8.66.

Regards:

Uwe Fechner