2007-04-20 3:23 AM
2011-05-17 12:39 AM
I would like to know if some one have try to implements an OFDM modulation using for examples an STR9. I see that it can perform an 256Point FTT in about 200us.
I see also that this device have an 10Bits A2D with a convertion time of 1uS.Is possible in some way to increase the ''sensibility'' form 10bits to 12Bits?2011-05-17 12:39 AM
Actually, I've got the same problem. I'd like to control a robot using WLAN ieee 802.11 b. I know I have to modulate somehow signal from MAC unit though I don't know signal parameters. I would appreciate the answer if there's on the market any baseband processor (for OFDM modulation and signal conditioning) so that I could easily connect my STR912 to such baseband processor and then to ZIF transceiver.Are there such devices on the market? If not then how to enable STR912 to communicate through WLAN - (WiFi)?