2005-04-29 02:23 AM
2005-04-29 02:23 AM
Hi,
I'm using the ST72F521R9 (TQFP64) with inDART-STX (+Demoboard) and I found a problem using Timer A interrupts (output compare feature): I've tested my code with STVD 3.1.1 and all works fine but, if I flash it (using DataBlaze), the TimerA interrupt handler is never called (although the application is running). Even if I debug it with SofTec STVD 3.0.0 (based on STVD 3.1.0) there's no way to have it working. Below the option bytes: [FMP_R] = Read-out protecion disabled [BIT1] package selection = 0 [VD] = Hi voltage threshold [CSS] = Enabled [WDG_SW] = Software [WDG_HALT] = No reset in halt [PLLOFF] = PLL disabled [OSCRANGE] = HS: 8-16 MHz [OSCTYPE] = Ext source [RSTC] = 4096 cycles [BIT15] package selection = 1 Does anyone know why? Previously, I've already used the same pieces of code (timerA interrupt etc...) in another application, with no problem... Thanks Regards Andrea