cancel
Showing results for 
Search instead for 
Did you mean: 

TIMER

dmerchez9
Associate II
Posted on April 29, 2005 at 13:28

TIMER

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dmerchez9
Associate II
Posted on April 29, 2005 at 12:02

Hello everybody!

I want to know if it's possible to use an internal timer not being obliged to reserve 4pins on the STR710F?

hichem2
Associate II
Posted on April 29, 2005 at 12:39

Hello Merchez,

Normally in STR71x familly you have an internal timer, it consists of a 16-bit counter driven by a programmable prescaler.

It may be used for a variety of purposes.

I cant understand what do you say by using 4pins on the STR710F?? and wich pins can be used, you think?

With regards,

Hich :-]

dmerchez9
Associate II
Posted on April 29, 2005 at 12:45

Hi

Is the internal timer the same as the timer3, timer2, timer1, or timer0?

Because for example timer3 is on pins 71, 72, 73, 74!

So if i use the internal timer, do i have to reserve those pins to make my timer running, or not?

regards

Dam

hichem2
Associate II
Posted on April 29, 2005 at 13:28

Hi,

Using the STR71x timer, you are not obliged to keep those pins reserved.

Cheers,

Hich ;)